ニュースとイベント

 

CUI Expands Custom Power Capabilities

With the recent asset acquisition of Tectrol, Inc. and its 74,000 sq. ft. design and manufacturing center in Toronto, CUI has greatly expanded its custom power capabilities.The organization is now positioned to be one of the most collaborative custom power supply partners in the industry.With over 1,500 field-proven custom designs and in-house capabilities from quick-turn prototypes to full-production, CUI's ability to manage design changes, schedule adjustments and control inventory makes the ideal partner for a range of custom power needs.

▶ Learn More

 

CUI、2015年度ECN Impact Awardsの2部門で最終選考に残る

CUI and its industry leading products have been announced as finalists in two separate categories for the 2015 ECN Impact Awards.この賞では、設計エンジニアリング業界で最も優れた、最も革新的な企業が表彰されます。CUI's rugged, high accuracy AMT31 commutation encoder series was named as a finalist for the Electromechanical/Mechanical Devices category, while its NDM3ZS-60 digital POL series was named a finalist in the Power Sources and Conditioning Devices category.

▶ Read the Press Release

 

New Products

ミッションクリティカルな(N+1)冗長アプリケーションに最適な3,000Wのフロントエンド電源

PSE-3000-48ファミリーは33.48W/立法インチの電力密度を実現し、40.64 x 101.6 x 355.6mmのコンパクトな標準1Uパッケージで、プラチナ・グレードの効率を達成しています。PSE-3000-48ファミリは48 Vdc出力にプリセットされていますが、42V~55Vの範囲で出力を調整でき、ワイヤレスや放送用アプリケーションに対応できます。AC、DC、I/O信号をすべて1つのコネクターに統合することで、ホットスワップのブラインドドッキング機能が実装されています。An optional 1U 19" power shelf is available to hold up to 4 power supplies for 12 KW parallel operation, 9 KW N+1 redundant operation, or dual 6 KW "A" & "B" output channel operation.

PSE-3000-48シリーズ

90 A Digital Point-of-Load (POL) Module Series to Addresses Growing Challenge of Powering Advanced ICs

The NDM3Z-90 family is the latest generation of digital POL modules from CUI's Novum® group.Designed specifically to address the increasing current needs of the latest processors, FPGAs and other advanced integrated circuits, the NDM3Z-90 sets new benchmarks in current density and efficiency.Rated to output 90 A, this family packs more power into a non-isolated module than anything else on the market.

  • クラス最高の効率
  • 優れた過渡応答
  • Compensation free design – always stable
  • Active current sharing, up to 4 modules at 360 A
  • Monitoring, communication and control via PMBus™
  • Architects of Modern Power™ (AMP Group) teraAMP™ compatible

NDM3Z-90シリーズ

CUI's Desktop External Ac-Dc Power Supply Series Expands to Meet Level VI Efficiency Standards

The SDI90-U and SDI120-U feature active power factor correction, a range of safety approvals and no-load power consumption less than 0.21 W. The 90 W and 120 W desktop adapters are the ideal solution to keep you one step ahead of the latest power regulations set to go into effect in February of 2016.

  • Up to 120 W continuous power
  • レベルVI対応の効率
  • ユニバーサル入力電圧範囲
  • 力率補正
  • No load power consumption < 0.21 W
  • 過電圧および短絡に対する保護機能を搭載
  • UL/cUL、GS、およびPSEの安全認証取得

SDI90-U Series / SDI120-U Series

Contest

CUI's AMT Family is a range of rugged, high accuracy modular encoders available in incremental, absolute, and commutation versions.その革新的な設計により、AMTシリーズは、産業環境でエンコーダーが受けることが多い汚染物質(汚れ、埃、油など)の影響を受けにくくなっています。

-40~+125°Cの動作温度、高精度、簡単な組み立て、低消費電流を兼ね備えたAMTは、産業、オートメーション、ロボティクス、再生可能エネルギーのさまざまなアプリケーションに対応する強力なソリューションとなります。

Question:Which two AMT Encoder Series incorporate the One Touch Zero™ feature?

Submit your answer to contest@cui.com

(Five winners will be selected on 2015年6月1日.Winners will be notified via email.)

リソース

APEC 2015 Video

CUI's Senior Vice President, Mark Adams, discusses the company's Novum® Advanced Power line including the newly released 90 A digital POL module, the company's acquisition of Canadian power supply company Tectrol, Inc., and the Architects of Modern Power™ consortium.

Watch It Now

Design World Level VI Article

Lee Teschler of Design World discusses the upcoming Level VI regulations including quotes from CUI's Product Manager for External Adapters, Andrew Johnson.

Read It Now

20050 SW 112th Avenue
Tualatin, OR 97062
1-800-275-4899
www.cui.com

            

 

Powered By OneLink