CUI's AMT11 Encoder Shortlisted for Elektra Awards 2014

2014年9月17日


CUI's AMT11 Encoder Shortlisted for Elektra Awards 2014

CUI's AMT11 modular incremental encoder has been shortlisted as a finalist for the Passive and Electromechanical Product of the Year as a part of Elektra Awards 2014.この賞の最終選考製品はすべて、設計、材料の使用、パッケージング技術において高いレベルにあることが示されました。今年は、かなりの数の企業が製品の発売、ビジネス・イニシアチブ、業績を掲げ、この賞にエントリーしました。審査団が最も強い印象を受けたエントリー候補が賞に選定されました。

CUI's AMT11 encoder offers the best of both worlds as a rugged, high accuracy solution for a range of applications.その革新的な設計により、AMTシリーズは、産業環境でエンコーダーが受けることが多い汚染物質(汚れ、埃、油など)の影響を受けにくくなっています。AMTの設計により、組み立て工程が単純化され、時間のかかる搭載・調整作業も数分で行うことができるようになりました。Combined with an operating temperature range up to -40°C to 125°C, high accuracy, a compact package, and low current draw, the AMT provides a compelling solution for motion control applications without the need to compromise.

The overall winners in each category will be announced at an Elektra Awards Dinner which takes place on Wednesday November 26 at the Lancaster London.

Additional information about Elektra Awards 2014 can be found here.

Learn more about CUI's AMT encoder series





 
Powered By OneLink